Summary (LTE-Advanced)
shows summary information about the Time Alignment Error (TAE) and Channel Power for each component carrier (CCx) relative to the selected Reference Component Carrier (Reference CC).
The for the CCx is calculated by subtracting the Time Offset of the reference CC from the Time Offset of the CCx.
The relative for the CCx is calculated by subtracting the Channel Power of the reference CC from the Channel Power of the CCx.
The shows either or . See the Cross-carrier In-band Emissions trace and Markers readout topics for more information.
- - The result will report the (the point at which the difference between the limit line and the emissions is smallest).
- - The result will report the (the point at which the difference between the limit line and the emissions that exceeded the limits is greatest).
See Also