About CW0/1 Decoded Symbol Tables
shows the decoded bits for the physical layer channels PBCH Physical Broadcast Channel, PDSCH Physical Downlink Shared Channel, PCFICH Physical Control Format Indicator Channel, and PDCCH Physical Downlink Control Channel for codeword 0. shows the decoded bits for PDSCH codeword 1. In addition, the bits for PBCH, PDCCH, and PCFICH codeword 0 are copied to to allow marker coupling.
The level of decoding is determined by the parameters on the Decode Tab. For more information about the bit format and contents, see one of the following topics:
The default bit order for this trace is MSB Most significant bit. In a binary coding scheme, the bit having the greatest numerical value. Analogous to the left-most numeric position in a decimal number.-first.
The channel bits are shown in the same order as on the DL Decode Info trace in each subframe.
Marker coupling between and other traces is at the subframe level.
The bits in this symbol table can be located outside the current range of bits shown. To view bits for a particular subframe:
-
Place a marker on the symbol table.
Right-click on the symbol table and click the marker visibility checkbox to display Marker 1.
-
Position the marker in the table and scroll to move the marker position to the desired location in the table.
Alternatively, you can double-click the subframe number in the marker readout window to open a dialog and edit the subframe position of the marker.
See Also