Decoded Symbol Table (LTE)
The shows decoded PUSCH Physical Uplink Shared Channel and PUCCH Physical Uplink Control Channel data. The PUCCH Bits and PUSCH Bits parameters define what level of decoding is performed.
The default bit order for this trace is MSB Most significant bit. In a binary coding scheme, the bit having the greatest numerical value. Analogous to the left-most numeric position in a decimal number.-first.
The bits for PUSCH and PUCCH allocations are shown in the same order as the corresponding decoded PUSCH and PUCCH information lines in the UL Decode Info trace.
Marker coupling between the and other traces is at the subframe level.
The bits in this symbol table can be located outside the current range of bits shown. To view bits for a particular subframe:
-
Place a marker on the symbol table.
Right-click on the symbol table and click the marker visibility checkbox to display Marker 1.
-
Position the marker in the table and scroll to move the marker position to the desired location in the table.
Alternatively, you can double-click the subframe number in the marker readout window to open a dialog and edit the subframe position of the marker.
See Also