Preset to Standard (LTE)
sets the demodulator to the specified bandwidth and sets the LTE Demod Properties dialog box parameters for the current direction (or ) to the default values listed in Using a Standard Setup.
Parameters not specific to the current direction are not changed. For example, when is set to downlink and the demodulator is preset to standard, uplink user allocations in the LTE Allocation Editor are left intact and will still be available when is switched back to uplink.
See Also