IQ Timing Skew (LTE)
is the time difference between the I and Q parts of the signal. This value is calculated for the entire signal in the Measurement Interval.
One possible cause of IQ timing skew is a difference in path length between the I and Q channels within the transmitter circuit.
The Measurement Interval must be longer than one symbol and contain at least one pair of subcarriers that are symmetric about DC for to be calculated.
For MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. signals, is shown on the MIMO Info Table under the IQTimSkew data result. The data result on the Error Summary Table will show "---" for multi-antenna signals.
See Also