Channel Power (LTE)
is the average power of the LTE Long Term Evolution signal and is calculated in the time domain over all symbols in the Measurement Interval.
For uplink, the 20 us transition periods before and after subframes (due to power steps or user allocation on/off transitions) are not included in the power calculation when Exclude EVM Transient Time is selected.
For downlink, is calculated from the reference measurement channel.
See Also