Decode PSDU (MB-OFDM)
Clear (See MB-OFDM Standard Setups/Presets Table.)
Select the checkbox to turn on decoding for the PSDU 1) PHY Service Data Unit, or 2) PLCP SDU (payload) bits.
The controls how complex the decoding algorithm should be with a range from 0 (low complexity) to 5 (high complexity). The default is 0. The results of the decoding are displayed in the PSDU Info Data trace. If is cleared, there will be no data in the PSDU Info Data trace.
Turning on the decoding will increase the measurement time. Higher may cause the measurement time to be extremely long.
See Also
Advanced Tab (MB-OFDM Demod Properties)