Lengths, Intervals, and Offsets  (MB-OFDM)

Menu Path: Analysis > MB-OFDM Demod Properties > Time tab

This topic describes the relationships between Search Length, Result Length, Measurement Interval, and Measurement Offset. It is the Measurement Interval and Measurement Offset parameters that define a specific interval within the Result Length for demodulation and analysis, where the Result Length pulse appears within the search time of the Search Length. These parameters allow quick analysis and viewing of specific time intervals of data because the VSA does not acquire new measurement data when the Measurement Interval or Measurement Offset is changed. When a new Measurement Interval or Measurement Offset is entered, the VSA re-computes the trace data results using the existing measurement data.

The following illustration displays the interrelationship between the parameters Search Length, Result Length, Measurement Interval, Measurement Offset, and PayLoad Octets. The Preamble plus the Result Length form the Packet Length, which is used for the Packet Time and Packet Spectrum traces. For more information, see MB-OFDM Packet.

See Also

MB-OFDM Modulation Overview

PayLoad Octet Calculations (MB-OFDM)

Using Standard Setups/Presets (MB-OFDM)

Format Tab (MB-OFDM Demod Properties)

Time Tab (MB-OFDM Demod Properties)

Advanced Tab (MB-OFDM Demod Properties)