Band Group (MB-OFDM)
(See MB-OFDM Standard Setups/Presets Table.)
1-6
specifies the band group of the signal. When this parameter is changed, the demodulator automatically sets the center frequency and span according to the band group specified. The demodulator also uses this parameter to determine which TFC Transport Format Combination hopping sequence table to use since the hopping sequences for band 5 are different from those for band groups 1-4 and 6. See MB-OFDM Modulation Overview Time-Frequency Codes section for more information.
See Also