Format Tab  (MB-OFDM)

Menu Path: Analysis > MB-OFDM Demod Properties > Format tab

The Format tab accesses the MB-OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. demodulation configuration parameters necessary for the VSA to lock on to and demodulate the test signal. Click on a parameter link for specific parameter information.

See Also

Time Tab (MB-OFDM Demod Properties)

Advanced Tab (MB-OFDM Demod Properties)

Packet Tab (MB-OFDM Demod Properties)