Post-Packet Time (MB-OFDM)

Menu Path: Analysis > MB-OFDM Demod Properties > Packet tab

Default: 0 (See MB-OFDM Standard Setups/Presets Table.)

Range: 0 to 20

Post-Packet Timedefines an additional processing time after the last symbol of the packet. Increasing Post-Packet Time allows time after the end of the packet to be analyzed for spectral issues. This setting applies to all the Band packet traces including the individual bands: Low | Mid | High Band Packet Time, Low | Mid | High Band Packet Spectrum and the composite band Packet Time and Packet Spectrum.

See Also

MB-OFDM Modulation Overview

Lengths, Intervals, and Offsets (MB-OFDM)

Using a Standard Setup (MB-OFDM)

Packet Tab (MB-OFDM Demod Properties)