Pre-Packet Time (MB-OFDM)

Menu Path: Analysis > MB-OFDM Demod Properties > Packet tab

Default: 0 symbol-times (See MB-OFDM Standard Setups/Presets Table.)

Range: 0 to 20 symbol-times

Pre-Packet Timedefines an additional processing time before the first symbol of the packet. Increasing this value allows the time prior to the beginning the packet for spectral issues to be analyzed. This setting applies to all the Band packet traces including the individual bands: Low | Mid | High Band Packet Time, Low | Mid | High Band Packet Spectrum and the composite band: Packet Time and Packet Spectrum.

See Also

MB-OFDM Modulation Overview

Lengths, Intervals, and Offsets (MB-OFDM)

Using Standard Setups/Presets (MB-OFDM)

Packet Tab (MB-OFDM Demod Properties)