MB-OFDM Demod Properties Dialog Box

Menu Path: Analysis > MB-OFDM Demod Properties

The MB-OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. Demod Properties dialog box contains parameters that configure the VSA to demodulate MB-OFDM modulated signals. The MB-OFDM demodulator must be selected before this dialog box is available (Analysis > Type > Other standard formats > Ultra Wideband MB-OFDM).

The MB-OFDM Demod Properties dialog box contains the following property tabs:

See Also

Setting up a MB-OFDM Measurement

Using Standard Setups/Presets (MB-OFDM)