CDF (MB-OFDM)
Menu Path:
The (Cumulative Distribution Function) trace shows the CDF Cumulative Distribution Function: The cumulative probability that a parameter will be less than a given value X. for the selected input channel. is computed by integrating the (Probability Density Function) of the OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. burst specified by the Measurement Interval and Measurement Offset. If the Offset is zero and the Interval is equal to the result length, the burst preamble is included in the CDF.
is the complement of and is defined as follows:
See Also
Available Trace Data (MB-OFDM)