Measurement Offset (MB-OFDM)

Menu Path: Analysis > MB-OFDM Demod Properties > Time tab

Default: 0 symbol-times (See MB-OFDM Standard Setups/Presets Table.)

Range: 0 to [variable depending on Result Length]

Measurement Offsetsets the start position of the Measurement Interval within the Result Length. To review the Search Length, Result Length, Measurement Offset, and Measurement Interval actions and interactions, see Lengths, Intervals, and Offsets.

See Also

MB-OFDM Modulation Overview

Lengths, Intervals, and Offsets (MB-OFDM)

Using Standard Setups/Presets (MB-OFDM)

Time Tab (MB-OFDM Demod Properties)