Sequenced Recording Playback (Measurements tab)
Sequenced Recording Playback specifies the mode used for sequencing measurements using recording playback. Sequenced Recording Playback is available when Acquisition Mode is set to Sequenced, and when at least two measurements use Data From Recording.
The VSA provides two Sequenced Recording Playback modes:
-
: (Default) Backwards-compatible, independent management of recording playback per measurement.
-
: During sequencing, any measurement to be run will be skipped except the measurement with the current position earliest in the recording. This is a coupling of measurements based on the current playback position (relative to playback start position) of each measurement (does not consider the recording timestamp).
The most restrictive stop-start playback properties across the measurements will determine the wraparound points for playback position of all playback measurements.
See Also
Use Cases for Multi-Measurement