Use Cases for Multi-Measurement Capability
There are many ways to use the Multi-Measurement capability provided by the 89600 VSA. The following is a list of use cases with a summary and a link to more information.
|
Use case |
Summary |
Benefits |
|---|---|---|
| Multi-Carrier Signal |
Multiple carriers from an MCPA (multi-carrier power amplifier) containing the same modulation format. Acquisition:Phase-Synchronous |
|
| Multi-Format Signal |
Multiple carriers containing different modulation formats, such as from a multi-standard radio. Acquisition:Time-Synchronous |
Single instrument
Multiple instruments
|
|
Analyze uplink and downlink frames and compare relative timing, power, etc. Acquisition: Phase-Synchronous |
|
|
| COMMS system Multiple test points |
Analyze the signal at different points in the RF Radio Frequency: A generic term for radio-based technologies, operating between the Low Frequency range (30k Hz) and the Extra High Frequency range (300 GHz). path of your transmitter. Acquisition: Time-Synchronous |
|
| Conflicting requirements |
Conflicting measurement requirements, such as wide Span and narrow ResBW or Vector vs. Demod. Acquisition: Phase-Synchronous |
|
| Sequenced Measurements |
Automatic sequencing of measurements. Acquisition: Non-Synchronous |
|
See Also