RS Rx. Power (Avg) (NB-IoT)
Menu Path:
is a linear average of the power of all narrowband RS resource elements from antenna port 0 and antenna port 1 (when present) over the data in the Measurement Interval.
can be used to calculate NRSRP as defined in Section 5.1.26 of 3GPP TS Technical Specification 36.214.
When there are multiple Rx channels present that contain transmissions from antenna port 0 or 1, the average NRS power is calculated for each Rx channel and added together to compute .
See Also