RSEVM (NB-IoT)
shows the average error vector magnitude of the narrowband reference signal for each NRS/Rx path and is calculated from the data in the Measurement Interval.
The NRS subcarrier EVMs are calculated and expressed relative to the average power of the signal. Then the EVMs are RMS averaged, and the result is expressed in dB or percentage depending on the Report EVM in dB parameter.
is calculated with a Symbol Timing Adjust setting of . When is set to a value other than , may not match the corresponding RS EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. in the Frame Summary table.
See Also