PDCCH (5G NR/5G-Advanced)
The panel contains the available parameters for one or more PDCCH.
PDCCH Channel Configuration
Add PDCCH - Adds a PDCCH to the transmission. When a PDCCH is added, a representative button is added at the top of the PDCCH parameter group.
Remove PDCCH - Removes the selected PDCCH.
Clear All - Removes all but the original PDCCH.
Enable Channels... - Quickly enables and disables the configured PDCCHs in a single dialog. You can also enable channels individually using the Enabled checkbox at the top of each PDCCH.
Search Space Mode Enabled - Enables or disables the use of user-defined search spaces for PDCCH resource allocation.
Enabled - Each PDCCH will use a user-defined search space which is identified by the PDCCH's Search Space Index parameter.
Disabled - User-defined search spaces are disabled and resource allocation is configured within each PDCCH.
Default: Disabled
PDCCH
Enabled - Enables or disables the selected PDCCH. You can also control all configured PDCCHs using the Enabled Channels dialog.
Default: Disabled
3GPP Version - Determines the 3GPP standard the PDCCH is compliant with.
R18 Latest (2023-12) - Interprets the PDCCH in compliance with R18 as of 2023-12
18.1.0 (2023-12) - Interprets the PDCCH according to version 18.1.0 of 38.211 (2023-12)
17.4.0 (2023-01) - Interprets the PDCCH according to version 17.4.0 of 38.211 (2023-01)
17.3.0 (2022-09) - Interprets the PDCCH according to version 17.3.0 of 38.211 (2022-09)
16.8.0 (2021-12) - Interprets the PDCCH according to version 16.8.0 of 38.211 (2021-12)
16.5.0 (2021-03) - Interprets the PDCCH according to version 16.5.0 of 38.211 (2021-03)
16.2.0 (2020-06) - Interprets the PDCCH according to version 16.2.0 of 38.211 (2020-06)
16.1.0 (2020-03) - Interprets the PDCCH according to version 16.1.0 of 38.211 (2020-03)
15.8.0 (2019-12) - Interprets the PDCCH according to version 15.8.0 of 38.211 (2019-12)
15.6.0 (2019-06) - Interprets the PDCCH according to version 15.6.0 of 38.211 (2019-06)
15.5.0 (2019-03) - Interprets the PDCCH according to version 15.5.0 of 38.211 (2019-03)
15.4.0 (2018-12) - Interprets the PDCCH according to version 15.4.0 of 38.211 (2018-12)
15.3.0 (2018-09) - Interprets the PDCCH according to version 15.3.0 of 38.211 (2018-09)
Default: R18 Latest (2023-12)
Choices: R18 Latest (2023-12), 18.1.0 (2023-12), 17.4.0 (2023-01), 17.3.0 (2022-09), 16.8.0 (2021-12), 16.5.0 (2021-03), 16.2.0 (2020-06), 16.1.0 (2020-03), 15.8.0 (2019-12), 15.6.0 (2019-06), 15.5.0 (2019-03), 15.4.0 (2018-12), 15.3.0 (2018-09)
RNTI Type - Sets the RNTI for the physical channel.
Default: C-RNTI
Choices: SI Status Indicator-RNTI, P-RNTI, RA 1) Random Access, or 2) Receiver Address-RNTI, Temp C-RNTI, C-RNTI, MCS modulation and coding scheme-C-RNTI, CS-RNTI, TPC Transmit Power Control-PUCCH-RNTI, TPC-PUSCH-RNTI, TPC-SRS-RNTI, INT-RNTI, SFI-RNTI, SP-CSI channel state information-RNTI
RNTI - RNTI is used for the scrambling for PDCCH CRC Cyclic Redundancy Check parity bits.
Default: 1
Range: 0-65535
C-RNTI - Sets the C-RNTI for the physical channel. C-RNTI is used for RRC connection and SPS scheduling.
Default: 1
Range: 0-65535
Power Boosting - Sets the relative power boosting (in dB) of the PDCCH physical channel.
Default: 0 dB
DMRS Power Boosting - Sets the relative power boosting (in dB) of the DMRS associated with this physical channel.
Default: 0 dB
Payload
Payload Size - Sets the payload size for the selected PDCCH physical channel.
Default: 20
DCI Format - Selects the Downlink Control Information format for the selected PDCCH. Refer to the 5G NR standard (38.212 - 7.3) for more information.
Default: Unsupported
Choices: Format0_0, Format0_1, Format1_0, Format1_1, Unsupported
Resource Allocation
Search Space Index - Sets the index of the desired search space for the selected PDCCH. Search spaces are defined using the PDCCH Search Spaces group of editing tools and parameters.
This setting is only available when Search Space Mode is enabled.
Default: 0
Range: 0-(depends on the number of defined search spaces)
CORESET ID - Sets the CORESET ID for the selected search space. CORESETs are defined in the BWP tab.
When Search Space Mode is enabled, CORESET ID is set within each search space.
According to the 5G NR standard, the controlResourceSetId (CORESET ID) is used with with other CORESET/search space/PDCCH parameters to calculate the CCE indexes of the PDCCH mapping.
Default: 1
Range: 1 to (depends on the number of defined CORESETs)
Manual CCE Offset - Enables or disables manual entry of CCE Offset. When enabled, manually set the CCE Offset (the DCI starting point). When disabled, CCE Offset is calculated based on slot index, Search Space Type, Aggregation Level, number of PDCCH candidates and Candidate Index.
Default: Disabled, 4
Search Space Type - Sets the type of the selected search space.
When Search Space Mode is enabled, Search Space Type is set within each search space.
Default: UE User Equipment (e.g. cell phone)-Specific
Range: UE-Specific, Common
Aggregation Level (L) - Sets the aggregation level for the selected PDCCH.
When Search Space Mode is enabled, Aggregation Level (L) selects the aggregation level to use for the selected search space (Search Space Index). Each aggregation level has an assigned PDCCH candidate number for each search space (default PDCCH Candidate Number = 4). This provides unlimited flexibility in configuring multiple search spaces for use with multiple PDCCHs.
Default: 1
Choices: 1, 2, 4, 8, 16
Symbol Start - Sets the starting symbol for the selected search space.
When Search Space Mode is enabled, Symbol Start is set within each search space.
Default: 0
Candidate Number - Sets the PDCCH candidate number to use for the selected Aggregation Level (L).
When Search Space Mode is enabled, the candidate number is set within each search space.
Default: 4
Choices:0, 1, 2, 3, 4, 5, 6, 8
Frame Period - The Frame Period parameter allows you to allocate each PDCCH over a specified number of frames (or frame period), providing the ability to define PDCCH patterns within the transmission. A PDCCH may be allocated to the same slot(s) in every frame of the transmission, or it may be allocated to various slots and frames.
When Frame Period is set to 1 and Numerology is set to 30 kHz kiloHertz: A radio frequency measurement (one kilohertz = one thousand cycles per second). subcarrier spacing (default), there are 20 slots and the PDCCH will appear in the same slot(s) in every frame. When Frame Period is set to 2, the range of the Allocated Slots parameter is 40 slots, and the PDCCH will appear in the allocated slots in every two frames. For each PDCCH, you can configure an allocated slot pattern up to 16 frames in length.
When Search Space Mode is enabled, frame period is set within each search space.
Default: 1 Frame
Range: 1-16
Allocated Slots - Specifies the slot(s) that contain the selected PDCCH. Allocated Slots are entered as an array of slot indexes.
The range of slots depends on the specified Frame Period and the Numerology. For 30 kHz subcarrier spacing, each frame consists of 20 slots. Setting Frame Period to 2 increases the Allocated Slots range to 40 slots.
Example:
Numerology = µ1 (30 kHz)
Selected PDCCH = PDCCH0
Frame Period = 2 Frames
Allocated Slots range: 0-39 (two frames)
Allocated Slots = 0, 2:4
Slots 0, 2, 3 and 4 are allocated for PDCCH0
PDCCH0 skips every other frame (slots 20-39)
Slots 1 and 5-39 are not allocated for PDCCH0. They can be allocated by other PDCCHs
When Search Space Mode is enabled, allocated slots are set within each search space.
Default: 0:19 (Frame Period = 1 Frame, 30 kHz subcarrier spacing)
Range: Maximum slot duration depends on the Numerology and Frame Period
Candidate Index - Sets the starting index for the selected PDCCH.
When Search Space Mode is enabled, Slot Format is set within each search space.
Default: 0
Slot Format - Sets the slot format used for the PDCCH.
|
3GPP Version 15.1.0 (2018-03) and later |
||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
Format |
Symbol number in a slot |
|||||||||||||||
| 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 | 8 | 9 | 10 | 11 | 12 | 13 | |||
| 0 | D | D | D | D | D | D | D | D | D | D | D | D | D | D | ||
| 1 | U | U | U | U | U | U | U | U | U | U | U | U | U | U | ||
| 2 | X | X | X | X | X | X | X | X | X | X | X | X | X | X | ||
| 3 | D | D | D | D | D | D | D | D | D | D | D | D | D | X | ||
| 4 | D | D | D | D | D | D | D | D | D | D | D | D | X | X | ||
| 5 | D | D | D | D | D | D | D | D | D | D | D | X | X | X | ||
| 6 | D | D | D | D | D | D | D | D | D | D | X | X | X | X | ||
| 7 | D | D | D | D | D | D | D | D | D | X | X | X | X | X | ||
| 8 | X | X | X | X | X | X | X | X | X | X | X | X | X | U | ||
| 9 | X | X | X | X | X | X | X | X | X | X | X | X | U | U | ||
| 10 | X | U | U | U | U | U | U | U | U | U | U | U | U | U | ||
| 11 | X | X | U | U | U | U | U | U | U | U | U | U | U | U | ||
| 12 | X | X | X | U | U | U | U | U | U | U | U | U | U | U | ||
| 13 | X | X | X | X | U | U | U | U | U | U | U | U | U | U | ||
| 14 | X | X | X | X | X | U | U | U | U | U | U | U | U | U | ||
| 15 | X | X | X | X | X | X | U | U | U | U | U | U | U | U | ||
| 16 | D | X | X | X | X | X | X | X | X | X | X | X | X | X | ||
| 17 | D | D | X | X | X | X | X | X | X | X | X | X | X | X | ||
| 18 | D | D | D | X | X | X | X | X | X | X | X | X | X | X | ||
| 19 | D | X | X | X | X | X | X | X | X | X | X | X | X | U | ||
| 20 | D | D | X | X | X | X | X | X | X | X | X | X | X | U | ||
| 21 | D | D | D | X | X | X | X | X | X | X | X | X | X | U | ||
| 22 | D | X | X | X | X | X | X | X | X | X | X | X | U | U | ||
| 23 | D | D | X | X | X | X | X | X | X | X | X | X | U | U | ||
| 24 | D | D | D | X | X | X | X | X | X | X | X | X | U | U | ||
| 25 | D | X | X | X | X | X | X | X | X | X | X | U | U | U | ||
| 26 | D | D | X | X | X | X | X | X | X | X | X | U | U | U | ||
| 27 | D | D | D | X | X | X | X | X | X | X | X | U | U | U | ||
| 28 | D | D | D | D | D | D | D | D | D | D | D | D | X | U | ||
| 29 | D | D | D | D | D | D | D | D | D | D | D | X | X | U | ||
| 30 | D | D | D | D | D | D | D | D | D | D | X | X | X | U | ||
| 31 | D | D | D | D | D | D | D | D | D | D | D | X | U | U | ||
| 32 | D | D | D | D | D | D | D | D | D | D | X | X | U | U | ||
| 33 | D | D | D | D | D | D | D | D | D | X | X | X | U | U | ||
| 34 | D | X | U | U | U | U | U | U | U | U | U | U | U | U | ||
| 35 | D | D | X | U | U | U | U | U | U | U | U | U | U | U | ||
| 36 | D | D | D | X | U | U | U | U | U | U | U | U | U | U | ||
| 37 | D | X | X | U | U | U | U | U | U | U | U | U | U | U | ||
| 38 | D | D | X | X | U | U | U | U | U | U | U | U | U | U | ||
| 39 | D | D | D | X | X | U | U | U | U | U | U | U | U | U | ||
| 40 | D | X | X | X | U | U | U | U | U | U | U | U | U | U | ||
| 41 | D | D | X | X | X | U | U | U | U | U | U | U | U | U | ||
| 42 | D | D | D | X | X | X | U | U | U | U | U | U | U | U | ||
| 43 | D | D | D | D | D | D | D | D | D | X | X | X | X | U | ||
| 44 | D | D | D | D | D | D | X | X | X | X | X | X | U | U | ||
| 45 | D | D | D | D | D | D | X | X | U | U | U | U | U | U | ||
| 46 | D | D | D | D | D | X | U | D | D | D | D | D | X | U | ||
| 47 | D | D | X | U | U | U | U | D | D | X | U | U | U | U | ||
| 48 | D | X | U | U | U | U | U | D | X | U | U | U | U | U | ||
| 49 | D | D | D | D | X | X | U | D | D | D | D | X | X | U | ||
| 50 | D | D | X | X | U | U | U | D | D | X | X | U | U | U | ||
| 51 | D | X | X | U | U | U | U | D | X | X | U | U | U | U | ||
| 52 | D | X | X | X | X | X | U | D | X | X | X | X | X | U | ||
| 53 | D | D | X | X | X | X | U | D | D | X | X | X | X | U | ||
| 54 | X | X | X | X | X | X | X | D | D | D | D | D | D | D | ||
| 55 | D | D | X | X | X | U | U | U | D | D | D | D | D | D | ||
| 56 | Reserved | |||||||||||||||
| 57 | Reserved | |||||||||||||||
| 58 | Reserved | |||||||||||||||
| 59 | Reserved | |||||||||||||||
| 60 | Reserved | |||||||||||||||
| 61 | Reserved | |||||||||||||||
| 62 - 255 | Reserved | |||||||||||||||
Default: 0: D,D,D,D,D,D,D,D,D,D,D,D,D,D
Search Spaces
Add SEARCH SPACE - Adds a user-definable search space. When a search space is added, a representative button is added at the top of the Search Space parameter group.
Remove SEARCH SPACE - Removes the selected search space.
SEARCH SPACE:
CORESET ID - Sets the CORESET ID for the selected search space. CORESETs are defined in the BWP tab.
According to the 5G NR standard, the controlResourceSetId (CORESET ID) is used with with other CORESET/search space/PDCCH parameters to calculate the CCE indexes of the PDCCH mapping.
When Search Space Mode is disabled, CORESET ID is set in the PDCCH Resource Allocation parameter group.
Default: 1
Range: 1 to (depends on the number of defined CORESETs)
Search Space Type - Sets the type of the selected search space.
When Search Space Mode is disabled, Search Space Type is set in the PDCCH Resource Allocation parameter group.
Default: UE-Specific
Range: UE-Specific, Common
Frame Period - The Frame Period parameter allows you to allocate each PDCCH over a specified number of frames (or frame period), providing the ability to define complex PDCCH patterns within the transmission. A PDCCH may be allocated to the same slot(s) in every frame of the transmission, or it may be allocated to various slots and frames.
When Frame Period is set to 1, the range of the Allocated Slots parameter is 0-19 (20 slots) and the PDCCH will appear in the same slot(s) in every frame. When Frame Period is set to 2, the range of the Allocated Slots parameter is 0-39, or 40 slots (two frames in length), and the PDCCH will appear in the allocated slots in every two frames. For each PDCCH, you can configure an allocated slot pattern up to 16 frames (320 slots) in length.
When Search Space Mode is disabled, frame period is set in the PDCCH Resource Allocation parameter group.
Default: 1 Frame
Default: 1-16
Allocated Slots - Specifies the slot(s) that contain the selected PDCCH. Allocated Slots are entered as an array of slot indexes.
The range of slots depends on the specified Frame Period. Each frame consists of 20 slots. Setting Frame Period to 2 increases the Allocated Slots range to 40 slots (0:39).
Example:
Selected PDCCH = PDCCH0
Frame Period = 2 Frames
Allocated Slots range: 0-39 (two frames)
Allocated Slots = 0, 2:4
Slots 0, 2, 3 and 4 are allocated for PDCCH0
PDCCH0 skips every other frame (slots 20-39)
Slots 1 and 5-39 are not allocated for PDCCH0. They can be allocated by other PDCCHs
When Search Space Mode is disabled, Symbol Start is set in the PDCCH Resource Allocation parameter group.
Default: 2:9, 12:19 (Frame Period = 1 Frame)
Range: Up to 320 slots (Frame Period = 16 Frames)
Symbol Start - Sets the starting symbol for the selected search space.
Default: 0
Slot Format - Sets the slot format used for the PDCCH.
When Search Space Mode is disabled, Slot Format is set in the PDCCH Resource Allocation parameter group.
|
3GPP Version 15.1.0 (2018-03) and later |
||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
Format |
Symbol number in a slot |
|||||||||||||||
| 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 | 8 | 9 | 10 | 11 | 12 | 13 | |||
| 0 | D | D | D | D | D | D | D | D | D | D | D | D | D | D | ||
| 1 | U | U | U | U | U | U | U | U | U | U | U | U | U | U | ||
| 2 | X | X | X | X | X | X | X | X | X | X | X | X | X | X | ||
| 3 | D | D | D | D | D | D | D | D | D | D | D | D | D | X | ||
| 4 | D | D | D | D | D | D | D | D | D | D | D | D | X | X | ||
| 5 | D | D | D | D | D | D | D | D | D | D | D | X | X | X | ||
| 6 | D | D | D | D | D | D | D | D | D | D | X | X | X | X | ||
| 7 | D | D | D | D | D | D | D | D | D | X | X | X | X | X | ||
| 8 | X | X | X | X | X | X | X | X | X | X | X | X | X | U | ||
| 9 | X | X | X | X | X | X | X | X | X | X | X | X | U | U | ||
| 10 | X | U | U | U | U | U | U | U | U | U | U | U | U | U | ||
| 11 | X | X | U | U | U | U | U | U | U | U | U | U | U | U | ||
| 12 | X | X | X | U | U | U | U | U | U | U | U | U | U | U | ||
| 13 | X | X | X | X | U | U | U | U | U | U | U | U | U | U | ||
| 14 | X | X | X | X | X | U | U | U | U | U | U | U | U | U | ||
| 15 | X | X | X | X | X | X | U | U | U | U | U | U | U | U | ||
| 16 | D | X | X | X | X | X | X | X | X | X | X | X | X | X | ||
| 17 | D | D | X | X | X | X | X | X | X | X | X | X | X | X | ||
| 18 | D | D | D | X | X | X | X | X | X | X | X | X | X | X | ||
| 19 | D | X | X | X | X | X | X | X | X | X | X | X | X | U | ||
| 20 | D | D | X | X | X | X | X | X | X | X | X | X | X | U | ||
| 21 | D | D | D | X | X | X | X | X | X | X | X | X | X | U | ||
| 22 | D | X | X | X | X | X | X | X | X | X | X | X | U | U | ||
| 23 | D | D | X | X | X | X | X | X | X | X | X | X | U | U | ||
| 24 | D | D | D | X | X | X | X | X | X | X | X | X | U | U | ||
| 25 | D | X | X | X | X | X | X | X | X | X | X | U | U | U | ||
| 26 | D | D | X | X | X | X | X | X | X | X | X | U | U | U | ||
| 27 | D | D | D | X | X | X | X | X | X | X | X | U | U | U | ||
| 28 | D | D | D | D | D | D | D | D | D | D | D | D | X | U | ||
| 29 | D | D | D | D | D | D | D | D | D | D | D | X | X | U | ||
| 30 | D | D | D | D | D | D | D | D | D | D | X | X | X | U | ||
| 31 | D | D | D | D | D | D | D | D | D | D | D | X | U | U | ||
| 32 | D | D | D | D | D | D | D | D | D | D | X | X | U | U | ||
| 33 | D | D | D | D | D | D | D | D | D | X | X | X | U | U | ||
| 34 | D | X | U | U | U | U | U | U | U | U | U | U | U | U | ||
| 35 | D | D | X | U | U | U | U | U | U | U | U | U | U | U | ||
| 36 | D | D | D | X | U | U | U | U | U | U | U | U | U | U | ||
| 37 | D | X | X | U | U | U | U | U | U | U | U | U | U | U | ||
| 38 | D | D | X | X | U | U | U | U | U | U | U | U | U | U | ||
| 39 | D | D | D | X | X | U | U | U | U | U | U | U | U | U | ||
| 40 | D | X | X | X | U | U | U | U | U | U | U | U | U | U | ||
| 41 | D | D | X | X | X | U | U | U | U | U | U | U | U | U | ||
| 42 | D | D | D | X | X | X | U | U | U | U | U | U | U | U | ||
| 43 | D | D | D | D | D | D | D | D | D | X | X | X | X | U | ||
| 44 | D | D | D | D | D | D | X | X | X | X | X | X | U | U | ||
| 45 | D | D | D | D | D | D | X | X | U | U | U | U | U | U | ||
| 46 | D | D | D | D | D | X | U | D | D | D | D | D | X | U | ||
| 47 | D | D | X | U | U | U | U | D | D | X | U | U | U | U | ||
| 48 | D | X | U | U | U | U | U | D | X | U | U | U | U | U | ||
| 49 | D | D | D | D | X | X | U | D | D | D | D | X | X | U | ||
| 50 | D | D | X | X | U | U | U | D | D | X | X | U | U | U | ||
| 51 | D | X | X | U | U | U | U | D | X | X | U | U | U | U | ||
| 52 | D | X | X | X | X | X | U | D | X | X | X | X | X | U | ||
| 53 | D | D | X | X | X | X | U | D | D | X | X | X | X | U | ||
| 54 | X | X | X | X | X | X | X | D | D | D | D | D | D | D | ||
| 55 | D | D | X | X | X | U | U | U | D | D | D | D | D | D | ||
| 56 | Reserved | |||||||||||||||
| 57 | Reserved | |||||||||||||||
| 58 | Reserved | |||||||||||||||
| 59 | Reserved | |||||||||||||||
| 60 | Reserved | |||||||||||||||
| 61 | Reserved | |||||||||||||||
| 62 - 255 | Reserved | |||||||||||||||
PDCCH Candidate Number:
When Search Space Mode is disabled, candidate number and aggregation level are set in the PDCCH Resource Allocation parameter group.
For Aggregation L1 - For the selected search space, PDCCH Candidate Number For Aggregation L1 sets the PDCCH candidate number to use when Aggregation Level L1 is selected for a PDCCH. Each PDCCH can have a different aggregation level, and each aggregation level can have a different PDCCH candidate assigned to it within a different search space using this group of settings.
Default: 4
Choices:0, 1, 2, 3, 4, 5, 6, 8
For Aggregation L2 - For the selected search space, PDCCH Candidate Number For Aggregation L2 sets the PDCCH candidate number to use when Aggregation Level L2 is selected for a PDCCH. Each PDCCH can have a different aggregation level, and each aggregation level can have a different PDCCH candidate assigned to it within a different search space using this group of settings.
Default: 4
Choices:0, 1, 2, 3, 4, 5, 6, 8
For Aggregation L4 - For the selected search space, PDCCH Candidate Number For Aggregation L4 sets the PDCCH candidate number to use when Aggregation Level L4 is selected for a PDCCH. Each PDCCH can have a different aggregation level, and each aggregation level can have a different PDCCH candidate assigned to it within a different search space using this group of settings.
Default: 4
Choices:0, 1, 2, 3, 4, 5, 6, 8
For Aggregation L8 - For the selected search space, PDCCH Candidate Number For Aggregation L8 sets the PDCCH candidate number to use when Aggregation Level L8 is selected for a PDCCH. Each PDCCH can have a different aggregation level, and each aggregation level can have a different PDCCH candidate assigned to it within a different search space using this group of settings.
Default: 4
Choices:0, 1, 2, 3, 4, 5, 6, 8
For Aggregation L16 - For the selected search space, PDCCH Candidate Number For Aggregation L16 sets the PDCCH candidate number to use when Aggregation Level L16 is selected for a PDCCH. Each PDCCH can have a different aggregation level, and each aggregation level can have a different PDCCH candidate assigned to it within a different search space using this group of settings.
Default: 4
Choices:0, 1, 2, 3, 4, 5, 6, 8
See Also
5G NR/5G-Advanced Demod Properties Dialog Box