Reference Channel (5G NR/5G-Advanced)
Reference Channel, along with Ref. Channel (under Channel), Ref. Antenna Port (under PDSCH, PUSCH, CSI-RS and SRS) and Channel ID (under Channel), defines which physical channel or signal, on which measurement channel and antenna port, is used as the reference when calculating the TAE and Phase Error results in the MIMO Info table and Beam Weights trace. See About Reference Channels with MIMO and Beamforming Measurements for more information and examples.
See Also