About DMRS MIMO Info Table (5G NR/5G-Advanced)

There are two types of traces in the Trace > Data > Demod and MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. menus that display component carrier data: CCn (component carrier is fixed), and Selected Display CC (component carrier is dynamically selected using the Display parameter). See About Per-Carrier Trace Types for more information.

The DMRS MIMO Info table shows a MIMO measurement's reference PDSCH Physical Downlink Shared Channel-DMRS or PUSCH-DMRS EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format., power, and time, frequency and phase offset for each antenna port.

The Ref. Channel parameter (under Channel) together with the Reference Channel setting (under Input & Antenna), the Ref. Antenna Port setting (under PDSCH and PUSCH) and the Channel ID setting (under Channel) defines which physical channel or signal, on which measurement channel and antenna port, is used as the reference when calculating the TAE and Phase Error results in the MIMO Info table and Beam Weights trace. See About Reference Channels with MIMO and Beamforming Measurements for more information and examples.

DMRS MIMO Info is a type of Matrix Table that provides sortable rows by column, selectable column visibility, and copy/paste and export functionality to share rows of content or complete tables to applications like email, text editing or spreadsheet programs.

The color coding used in the DMRS MIMO Info table coordinates with the physical channel color coding used in the Frame Summary table.

 

 

Not visible by default

To make visible, right-click any column heading and select Column Visibility...

             
Name Physical Channel User Part Meas. Channel Antenna Port Despread EVM (%rms) Power per RE (dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer) TAE (sec) Frequency Offset (Hz) Phase Offset (deg)

Downlink:

  • PDSCHn_DMRS

Uplink:

  • PUSCHn_DMRS

Downlink:

  • PDSCH

Uplink:

  • PUSCH

Downlink:

  • n

Uplink:

  • n

When there is a single user, the default user number is 0. Rows without user data are denoted with '***'.

Downlink:

  • DMRS

Uplink:

  • DMRS

Downlink:

  • Chn

Uplink:

  • Chn

Downlink:

  • Portn

Uplink:

  • Portn

Despread EVM represents the error present in the measured signal for a PDSCH-DMRS or PUSCH-DMRS channel for a particular input channel when code despreading is applied for a particular port.

The despreading operation isolated noise that is not correlated across subcarriers. For AWGN Additive White Gaussian Noise - Statistically random radio noise characterized by a wide frequency range with regards to a signal in a communications channel., this will lead to a -3 dB difference compared to PDSCH-DMRS or PUSCH-DMRS EVM shown in Frame Summary.

-------------------------------

Power per RE is the per-path power at each antenna port of the MIMO measurement.

TAE (Time Alignment Error) is the detected timing offset of the physical channel for each path. The reference is the reference antenna port DMRS signal measured on the reference measurement input channel.

Frequency Offset is the detected frequency offset of the physical channel for each path.

Frequency Offset is relative to the measurement center frequency.

Phase Offset is the detected phase offset of the physical channel for each path.

For Phase Offset, the reference is the reference antenna port DMRS signal measured on the reference measurement input channel.

n denotes the physical channel, measurement channel, user or antenna port number.

Averaging is not applied to the DMRS MIMO Info trace.

See Also

CSI-RS MIMO Info

Matrix Tables