Regions Tab (Pulse)

Menu Path: Analysis > Pulse Properties > Regions

The Regions tab lets you set thresholds, FM Frequency Modulation Filter bandwidth, and the pulse width for Frequency/Phase and Ripple calculations.

Thresholds

Analysis Regions

Spectrum Window -- Lets you specify among the following types of windows used for FFT analysis:

Max Spectrum FFT Fast Fourier Transform: A mathematical operation performed on a time-domain signal to yield the individual spectral components that constitute the signal. See Spectrum. Length -- Lets you set the maximum FFT length for the current measurement. Smaller FFT lengths result in faster measurements. Larger lengths give more precise frequency values.

See Also

Pulse Width

Amplitude Domain

Top/Base Calculation Method

Adjust Threshold For Droop

Assumed Pulse Modulation