Display Detection Threshold Line (Pulse)

Menu Path: Analysis > Pulse Properties > Pulse Detection

When the Display Detected Threshold Line checkbox is enabled, the Pulse Detection Threshold (dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer) level line is displayed within the Acquisition Time and Amplitude (Meas and Ref) trace results. The horizontal Pulse Detection Threshold (dBm) level line is identified within the trace results as “DET THRESH”.

When the Display Detected Threshold Line checkbox is disabled, no Pulse Detection Threshold (dBm) level line is displayed in results traces.

Note that the Pulse Detection Threshold (dBm) level is also reported as a numeric result within the Pulse Summary table, as “Detection Thresh”.