Amplitude Traces (Pulse)
You can select from the following amplitude traces when making Pulse Measurements:
- Amplitude Error Time (Channel 1)
- Amplitude Meas Time (Channels 1 and 2)
- Amplitude Ref Time (Channel 1)
- Instantaneous Amplitude Error Time (Channel 1)
- Instantaneous Amplitude Meas Time (Channels 1 and 2)
Note that Selected Pulses affects which pulses are displayed in the Amplitude, Phase, and FM Frequency Modulation traces.
See Also