FM Traces (Pulse)
You can select from the following FM Frequency Modulation Traces when making Pulse measurements:
- FM Error Spectrum (Channel 1)
- FM Error Time (Channel 1)
- FM Meas Spectrum (Channel 1)
- FM Meas Time (Channels 1 and 2)
- FM Ref Spectrum (Channel 1)
- FM Ref Time (Channel 1)
- Instantaneous FM Error Spectrum (Channel 1)
- Instantaneous FM Error Time (Channel 1)
- Instantaneous FM Meas Spectrum (Channel 1)
- Instantaneous FM Meas Time (Channels 1 and 2)
- FM Filter Coefs (Channel 1)
Note that Selected Pulses affects which pulses are displayed in the Amplitude, Phase, and FM traces.
See Also