CW Lower (RFID)
10% (See RFID Standard Setups/Presets Table)
0 to 90%
The setting sets the lower threshold for determining the rise and fall times for the CW signal.
Rise and fall times of the Interrogator CW signal are determined by two threshold levels, expressed as a percentage of the steady-state CW level.
See Also