Thresholds (RFID)
The area of the tab specifies several parameters that determine the rise and fall times for The CW and ASK signals.
The area contains five parameters:
ASK Thresholds vs. OOK Thresholds
The 0% point for the ASK lower threshold is different from the 0% point for OOK lower threshold. OOK 0% is defined as 0 V, but ASK 0% is defined as the lower amplitude level. This is shown in the following illustration:
See Also