CW Settling (RFID)
5% (See RFID Standard Setups/Presets Table)
0 to 50%
The setting ses the settling level of the Interrogator CW signal. The value is a percentage of the steady-state CW level. The CW signal is considered to be settled when it stays within the settling threshold of the steady-state CW level.
See Also