Summary NFC (RFID)
The table shows the results of RFID analysis signal parameters defined for Near Field Communications (NFC).
The trace title is determined by the type of modulation format specified by the Fwd Format or the Ret Format selected on the Format Tab on the dialog box. The trace title options are:
- ASK Summary NFC
- FSK Frequency Shift Keying: A form of modulation using multiple carrier frequencies to carry the digital information. The most common is the two frequency FSK system using the two frequencies to carry the binary ones and zeros. Summary NFC
- OOK Summary NFC
See Also