Slot Frequency Reference (TD-SCDMA)
Midamble (See TD-SCDMA Standard Setups/Presets Table.)
specifies whether the appropriate timeslot or the section of the timeslot will be used as the frequency and phase reference for an individual traffic timeslot.
The setting affects the displayed Composite Frequency Error, as well as results that depend on the rotation of the data symbols-the symbols (bits) and the sign of the Composite Gain Imbalance results.
If is selected and the appropriate pilot timeslot (UpPTS for an uplink timeslot) is not present, a warning is displayed. The Uplink Switch Point parameter sets which traffic timeslots are uplink and which are downlink.
See Also