Uplink Switch Point (TD-SCDMA)
0 (See TD-SCDMA Standard Setups/Presets Table.)
: 0 to 6
specifies which Traffic TimeSlots are uplink and which are downlink.
is the timeslot number of the last uplink traffic timeslot. Timeslots from the following (next higher numbered) traffic timeslot through the end of the sub-frame are treated as downlink timeslots.
See Also