Code Channel (TD-SCDMA)
0 (See TD-SCDMA Standard Setups/Presets Table.)
: 0 to "Spread Code Length – 1"
sets the Despread Channel . The Despread Channel is used, along with the Despread Channel Spread Code Length, to specify the active code channel and layer used for the channel trace data measurement results (including: , , , , , and trace data results).
Use the Copy Mkr To Despread Channel marker feature to automatically specify the and setting.
See Also