Spread Code Length Despread Channel (TD-SCDMA)
16 (80 ksyms/s) (See TD-SCDMA Standard Setups/Presets Table.)
: 1, 2, 4, 8, or 16
The Despread Channel is used, along with the Despread Channel Code Channel, to specify the active code layer and channel used for the channel trace data measurement results ( including: , , , Chan Mag Error, and trace data results).
Selecting Despread Channel Spread Code Length
Click one of the available TD-SCDMA compliant from the drop-down list.
Use the marker feature to automatically specify the Despread-Channel and Code Channel settings.
See Also