Uplink Pilot (TD-SCDMA)
0 (See TD-SCDMA Standard Setups/Presets Table.)
: 0 to 255
Uplink Pilot specifies the Uplink Pilot synchronization ID sequence (SYNC-UL Up Link (reverse link: from cell phone to base station)) (see TD-SCDMA - Code/ID Allocation Overview).
controls the allowable Uplink Pilot ID sequence coding criteria as follows:
: Only allows Uplink Pilot ID sequences that comply with standard coding allocation criteria.
: Allows non-standard Uplink Pilot ID sequence allocation.
See Also