Time Tab (TD-SCDMA)
The T tab of the dialog box configures the data analysis parameters. Use these parameters to specify what segment of the time record (captured input signal) will be used for data analysis and trace data results.
These parameters can be reconfigured to get new trace data results without acquiring new data. The new data results are recomputed from the current data record, except on the first occurrence. On the first occurrence, the trace data results are computed from the Analysis Timeslot and Analysis Sub-frame settings.
The Time tab configures these parameters (click on the parameter name for more information):
See Also
Channel/Layer Tab (TD-SCDMA Demod Properties)
Code/ID Tab (TD-SCDMA Demod Properties)
Format Tab (TD-SCDMA Demod Properties)