Include Sync/Pilot Symbols (TEDS)
Selected (See Using Standard Setups/Presets)
, when selected, includes synchronization and pilot symbols in Error Vector Magnitude (EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format.) calculations.
Synchronization and pilot symbols have magnitude "1" and appear on the sync/pilot locus of the constellation diagram at phase angles that correspond to the standards.
See Also