Despread Traces (W-CDMA(3GPP)/HSPA)
Normal (See W-CDMA(3GPP) Standard Setups/Presets Table.)
The Despread Channel - specifies the measurement Test Plane within the HSPA+MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. analysis signal flow for the Despread (x) category of Trace Data results, where (x) is the Despread category number (Despread 1, Despread 2, Despread (x)). Refer to the Available Trace Data (W-CDMA(3GPP)/HSPA) topic for list of . .
How to Make a HSPA+MIMO Despread (x) Trace Data measurement
To learn how to use the Despread Traces parameter to make a measurement, see HSPA+ MIMO Overview - Despread (x) Trace Data.
How to use the Despread Traces Parameter
To select a particular Despread (x) Category Trace Data result, first determine the appropriate HSPA+MIMO measurement Test Plane for the desired Despread (x) Trace Data result. Then use the "Despread Traces" property to configure the VSA for the measurement. The HSPA+MIMO Trace Mapping Diagram and Test Plane Location Mapping Table are used to determine the correct Despread measuremen HSPA+MIMO Test Plane. Go to the d topic for complete details about using the Despread Traces parameter to make Despread (x) Channel measurements
The Despread Traces Parameter Table is used to determine the correct Despread Traces parameter "HSPA+MIMO Test Plane" for a particlular Despread (x) Trace Data result. Use the reference and HSPA+ MIMO Trace Mapping Diagram to identify the Despread Trace Data measurement Test Plane Location for the desired Despread (x) Trace Data result.
Despread Traces Parameter Table
|
Despread Traces Parameter |
Despread 1 (Meas Test Plane Ref(2)) |
Despread 2 (Meas Test Plane Ref(2)) |
|---|---|---|
| Normal(1) | D1 | D2 |
| HS TrBlock | E1 | E2 |
| HS TrBlock1 per Antenna | F1 | F2 |
| HS TrBlock2 per Antenna | G1 | G2 |
|
Notes (1) When is selected, the Despread 1 traces map to the legacy "Channel 1 Chan" traces, and represent the measured data immediately after removing the orthogonal spreading code for a specific code channel (2) To view the measurement Test Plane Location within the HSPA+MIMO signal flow, locate the Meas Test Plane Reference in the HSPA+ MIMO Trace Mapping Diagram. |
||
property is only available for Downlink HSPA+MIMO Spread Code Length 16 (240.0 ksym/s), > 1 Antenna analysis.
Configure the VSA for HSPA+MIMO Analysis
To configure the VSA for Downlink HSPA+MIMO, Spread Code Length 16 (240.0 ksym/s), >1 Antenna measurement analysis, set the following VSA parameters:
- Select Direction: tab
- Select : tab
- Select of 2 (or more): tab
- Specify : tab
See Also