Number of Tx Antennas (W-CDMA(3GPP)/HSPA)
1 (See W-CDMA(3GPP) Standards Setups/Presets Table.)
parameter specifies the number of transmit antennas used by the device under test. Select 2 (or more) Tx Antennas to enables MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. transmission analysis.
| MIMO transmission analysis is not performed. | |
| MIMO tranmission analysis is performed. |
1) The parameter is only available when Direction and is selected.
2) The MIMO Parameters on the Demod Properties Advanced tab are only available for HSPA+MIMO signal analysis.
3) MIMO Anaysis Mode: To configure the VSA for HSPA+MIMO analysis, select Downlink direction, Enable HSPA analysis and specify Number of Tx Antennas for 2 (or more).
See Also