Despread Error Vector Time (W-CDMA(3GPP)/HSPA)

When W-CDMA(3GPP)/HSPA Demodulation is enabled, the Error Vector Time trace data shows the Time Domain error vector trace data results for the specified Code Channel and code layer (Spread Code Length). Error Vector Time trace data is the computed error vector between corresponding symbol points in the I/Q measured and I/Q reference signals. The data results can be viewed as Error Vector Magnitude, Error Vector Phase, only the I component or only the Q component (see Trace Data Formats below).

image\EVTime4_wmf.jpg

Increase the number of symbol points by increasing the Measurement Interval (see Measurement Interval).

If normalization is off, the VSA shows the instantaneous magnitude for each point. If normalization is on, the VSA shows the error vector as a percentage. (See Normalize IQ Traces for an explanation of how this percentage is derived).

Trace Data Formats

It is important to remember that the Error Vector Time trace is a time record made up of complex, time domain data. Each point in the time record has two components: I and Q. To make sense of the data, select an appropriate trace data format (Trace > Properties > Format > Format drop-down list).

For example, to see the error vector magnitude, select the Linear Mag trace format (Trace > Properties > Format > Format > Linear Mag). Selecting Linear Mag computes the square root of the sum of the squares for each complex pair of points in the time record, which is the error vector magnitude (EVM):

image\EVTime3_wmf.jpg

 

How to Make a HSPA+MIMO Despread (x) Trace Data measurement

To learn how to use the Despread Traces parameter to make a Despread (x) Channel Trace Data measurement, see HSPA+ MIMO Overview - Despread (x) Trace Data.

See Also

Despread Channel Trace Data

About Trace Data (W-CDMA(3GPP))