EVM (W-CDMA(3GPP)/HSPA)
is the Error Vector Magnitude for the specified Code Channel and Spread Code Length. The display shows these EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. values; the RMS (root mean square in percent) EVM, the Peak (largest) EVM, and the symbol number with the Peak EVM.
is similar to Digital Demod EVM. See Digital Demod Error Vector Magnitude (EVM) for further information about this trace data.
See Also
Digital Demod Error Vector Magnitude (EVM)