RCDE (W-CDMA(3GPP)/HSPA)
The result on the Despread Channel Syms/Errs table is computed according to TS34.121 and measured on the first slot of the Measurement Interval for the despread code channel. This is the same as the value presented in the Code Domain Offsets table for the despread code channel.
The despread code channel is specified by Code Channel and Spread Code Length.
Additional RCDE resuts
- Comp RCDE For 64QAM The Comp RCDE For 64QAM result (Composite Error Summary table trace) is the averaged Relative Code Domain Error result for all active 64QAM channels.
- RCDE for all active channels: The Code Domain Offsets table trace lists the RCDE for all active channels (and ) within the .
See Also