Measurement Interval (W-CDMA(3GPP)/HSPA)
1 Slots (See W-CDMA(3GPP) Standard Presets Table.)
specifies the time length of data within the acquired Result Length data that is used for analysis and displayed trace data results. is entered as an integer number of time Slots. One time slot is equal to 2560 chips and is equal to 666.7 µs at the default .
and parameters are used to specify what region of the data is used for data analysis (see About Measurement Interval and Offset).
See Also
About Measurement Interval and Offset