Time Tab (802.11b/g DSSS/CCK/PBCC)
The tab of the IEEE Institute of Electrical and Electronics Engineers. A US-based membership organisation that includes engineers, scientists, and students in electronics and related fields. The IEEE developed the 802 series wired and wireless LAN standards. Visit the IEEE at http://www.ieee.org 802.11b/g Demod Properties dialog box specifies the signal capture configuration parameters. These parameters are used to select the pulse search length and to isolate a segment of the time record for further viewing and data analysis.
The tab dialog box configures these parameters:
See Also
Advanced Tab (802.11b/g DSSS/CCK/PBCC)