Distributed RUs (802.11n/ac/ax/be/bn)

For 802.11bn with Allocation Mode set to Legacy, when the signal bandwidth is 80 MHz Megahertz: A unit of frequency equal to one million hertz or cycles per second. or greater, there will be parameters to specify the RU distribution for each 80 MHz subband.

See Allocation Signaling topic for examples on configuring DRU signals.

See Also

Format Tab

802.11n/ac/ax/be/bn Demod Properties