Measurement Channel Enable (802.11n/ac/ax/be/bn)

Measurement Channel Enable is similar to using the Acquisition > Channels menu to switch between 1, 2, ..., 8-channel measurements. However, Measurement Channel Enable provides faster switching and also enables only specific channels, if desired. For example, channel 3 can be the only channel enabled or both channel 2 and 4 can be enabled.

When the 802.11ac 80+80 MHz or 802.11ax 80+80 MHz standards are selected, the Measurement Channel Enable will always have exactly 2 measurement channels selected.

The Number of Spatial Streams parameter is limited in the 89600 VSA to one of two selections: either a single spatial stream, or the number of measurement channels enabled.

See Also

Format tab

802.11n/ac/ax/be/bn Demod Properties