TB PPDU Parameters (802.11n/ac/ax/be/bn)
TB PPDU 1) IEEE 802.11: PHY (formerly PLCP) protocol data unit or 2) DVB-RCS2 (RLE): payload adapted PDU Parameters need to be specified for a TB PPDU to be reliably demodulated and PSDU 1) PHY Service Data Unit, or 2) PLCP SDU bits decoded. Normally these parameters would be supplied by the EHT-SIG, but a TB frame does not contain EHT-SIG. This parameter group is available when TB (Trigger Based) PPDU is selected.
Other parameters that need to be supplied for successful decoding of a TB frame in Manual mode are the DCM (802.11ax only) and Coding parameters for each user.
Pre-FEC Forward Error Correction: An encoding technique that allows a limited number of errors in digital stream to be corrected based on knowledge of the encoding scheme used. Padding Factor - Sets the number of
See section 36.3.13.3.5 in 802.11be/D1.0 or section 27.3.11.2 in 802.11ax/D4.2 for implementation details.
Default: 1
Range: 1-4
Space Time Block Coding - indicates whether the signal has Space Time Block Coding enabled. This setting is only applicable to 802.11ax and when the number of channels (streams) = 2.
PE Disambiguity - sets the packet extension disambiguity value. Selected = 1, cleared = 0.
LDPC low-density parity check Extra Symbol Present - LDPC Extra Symbol Segment field value. Selected = 1, cleared = 0.
See Also