This topic discusses updates to the DataLink software.
- Updated:
- DANL (Displayed Average Noise Level) - to be used with the FieldFox's RTSA and SA modes. This feature is executed on the FieldFox PC via the Data Link software.
- Added: Can open SA and RTSA Autosession (n) files and apply markers and preferences and save as a data link save (*.dls) file
- Added: Can open data link save (*.dls) files without opening an RTSA/SA AutoSession.
- Improved: Preferences dialog box behavior.
- Added: Saving a user-defined Waterfall data area.
- Added: AutoSession (n) Report capability for better data tracking of an AutoSession.
- Added DANL (Displayed Average Noise Level) - to be used with the FieldFox's RTSA and SA modes. This feature is executed on the FieldFox PC via the Data Link software.
- Added: Can open SA and RTSA session *.csv files and apply markers and preferences and save as a data link save (*.dls) file
- Added Record / Playback - Trace Recording Tool. Enables you to convert your playback files to *.csv files.
- Added Viewing Playback Data topic
- Updated Open and Save Files topic - new content on SA and RTSA record/playback files.
- Open legacy CSV cable correction file into a file editor. This is an update from Datalink versions >5.17 and <6.2.
- Add a new tool to convert legacy CSV files to XML. Customer may prefer using Microsoft Excel to modify cable files, then convert the file to XML for use in Field Fox with latest firmware.
- Open XML cable correction file brings up an editor that allows customer to save the XML file as CSV file.
-- This conversion tool (new format xml convert to legacy format csv) might be useful for customers who can use Microsoft Excel to modify CSV files.
-- Might be useful for customer needing correction files that work on older Field Fox firmware versions.
Integrated VNA Cal Kit Editor - This Cal Kit Editor is used in other Keysight VNA models or as a stand-alone application. Among other new capabilities, it can be used to open and save Cal Kits that are used in other VNA models. The help file for the Cal Kit Editor can be viewed by clicking a help button on the Cal Kit pages.
Connect to N9923A and N9912A when using FieldFox firmware A.05.15
In CAT Mode Return Loss and DTF Measurement, returns both traces.
Captures DTF Markers