This command is replaced with CALCulate:LIMit:LLData which can also set Relative Limits. (Read-Write) Set and query the data to complete the limit line table. - For NA and CAT mode, this command operates on the selected trace. First select a trace using CALC:PAR<tr>:SELect. - For ACP measurements, use CALCulate:ACPower:OFFSet:LIST:LIMit:NEGative[:UPPer]:DATA and CALCulate:ACPower:OFFSet:LIST:LIMit:POSitive[:UPPer]:DATA. |
|||||||||||||
Relevant Modes |
|||||||||||||
Parameters |
|
||||||||||||
<data> |
Data for all limit segments in the following format:
Subsequent segments are appended to the data in the same manner. |
||||||||||||
Examples |
'The following writes three upper limit segments for a 40 MHz bandpass filter. ' individual segments are highlighted for readability. CALC:LIM:DATA 3,1,0,2e7,3e7,-30,0,1,0,3e7,5e7,0,0,1,0,5e7,6e7,0,-30 |
||||||||||||
Query Syntax |
CALCulate:LIMit:DATA? |
||||||||||||
Return Type |
Block data |
||||||||||||
Default |
0 - Limit line data off |
||||||||||||