(Read-Write) Set and query the Y-axis scale per division value. Use this command with DISPlay:WINDow:TRACe:Y[:SCALe]:RPOSition and DISPlay:WINDow:TRACe:Y[:SCALe]:RLEVel which establish the reference position and level. |
|
Relevant Modes |
CAT, EMI, NF, NA, SA, RTSA, FOPS CAT mode: This command always acts on the selected trace. Select a trace using CALCulate:PARameter:SELect SA mode: Applicable ONLY when [:SENSe]:AMPLitude:SCALe = LOG; (Units are always "dB") |
Parameters |
|
<n> |
NA mode Only: Specify the displayed trace number. Choose from 1 to 4. For NF mode Only: Specify the displayed trace number. Choose from 1 to 2. If unspecified, value is set to 1. |
<num> |
Scale value. Units depend on the selected format. |
Examples |
DISP:WIND:TRAC1:Y:PDIV -.25 |
Query Syntax |
DISPlay:WINDow:TRACe<n>:Y[:SCALe]:PDIVision? |
Return Type |
Numeric |
Default |
Depends on Mode |
Last Modified:
04no2022 |
Added EMI mode (12.3x) |
01june2018 |
Added NF mode Opt. 356 (10.3) |
10-june-2016 |
Added RTSA mode (9.50) |
19-Mar-2014 |
Added FOPS |
11-Nov-2013 |
Modified again |
26-Apr-2012 |
Modified for CAT (5.75) |